21.4.34 sd_instantiate_hdl_module
(Ask a Question)Description
This Tcl command instantiates a HDL module in a SmartDesign component. The HDL file in which the HDL module is defined must be imported/linked before running this command.
sd_instantiate_hdl_module -sd_name {smartdesign component name} \
                          -hdl_module_name {hdl module name} \
                          -hdl_file {hdl file} \
                          [-instance_name {instance name}]Arguments
| Parameter | Type | Description | 
|---|---|---|
sd_name  | string  | Specifies the name of the SmartDesign component. It is mandatory.  | 
hdl_module_name  | string  | Specifies the name of the HDL module being instantiated in the SmartDesign component. It is mandatory.  | 
hdl_file  | string  | Specifies the path of the HDL file in which the HDL module is defined. The HDL file path can be relative to project folder for imported files but the path has to be complete for linked files. It is mandatory.  | 
instance_name  | string  | Specifies the instance name of the HDL module. It is optional. By default, the instance name is <hdl_module_name>_<index> (index is an automatically generated integer starting at 0 such that the instance name is unique in the SmartDesign).  | 
| Return Type | Description | 
|---|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|---|
None  | Required parameter 'sd_name' is missing.  | 
None  | Required parameter 'hdl_file' is missing.  | 
None  | You cannot instantiate a sub-module 'module_name' of HDL module.  | 
None  | Parameter 'param_name' is not defined. Valid command formatting is 'sd_instantiate_hdl_module -sd_name "sd_name" [-hdl_module_name "hdl_module_name"] -hdl_file "hdl_file" [-instance_name "instance_name"]'.  | 
Supported Families
| Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
Example
The following example instantiates a 'top' module in a SmartDesign 'mydesign' component "top_0" instance name (by default):
sd_instantiate_hdl_module -sd_name {mydesign} \
                          -hdl_module_name {top} \
                          -hdl_file {hdl/top.v} \
                          -instance_name {}See Also
sd_instantiate_hdl_core
sd_instantiate_core