21.4.28 sd_disconnect_pins
(Ask a Question)Description
This Tcl command disconnects a list of SmartDesign top level ports and/or instance pins from the net they are connected to.
Note: This command is not required to build a SmartDesign component. It maps to an interactive user action in the SmartDesign Canvas and will not be present in the exported file when user selects Libero Project -'Export Component Description(Tcl)' on a SmartDesign component.
sd_disconnect_pins -sd_name {smartdesign component name} \
                   -pin_names {port or pin or slice names}Arguments
| Parameter | Type | Description | 
|---|---|---|
| sd_name | string | Specifies the name of the SmartDesign component. It is mandatory. | 
| pin_names | string | Specifies the port, pin and/or slice names to be disconnected as follows: {"instance_name:pin_name" "port_name"}. This command will fail if the ports, pins and/or slices do not exist. There may be multiple -pin_names arguments (see example below). This is mandatory. | 
| Return Type | Description | 
|---|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|---|
| None | Parameter 'pin_names' is missing or has invalid value. | 
| None | Required parameter 'sd_name' is missing. | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'sd_disconnect_pins -sd_name "sd_name" -pin_names "[pin_names]+"'. | 
SDCTRL05  | Pin 'pin_name' does not exist. | 
Supported Families
| Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
Example
The following command disconnects "B_ren" and "B_ADRR[12:12]" slice from the "SD1" design:
sd_disconnect_pins -sd_name {SD1} \ -pin_names {B_ren RAM1K20_0:B_ADRR[12:12]}The following command disconnects "AND2_0:B", "AND3_0:APF_XCVR_ERM_C0_0:LANE0_RX_READY" pin/ports from the "SD2" SmartDesign:
sd_disconnect_pins \ -sd_name {SD2} \ -pin_names {AND2_0:B AND3_0:APF_XCVR_ERM_C0_0:LANE0_RX_READY}
See Also
- sd_connect_pins