21.4.42 sd_rename_port
(Ask a Question)Description
This Tcl command renames a SmartDesign port name.
Important: This command is not required to build
                a SmartDesign component. It maps to an interactive user action in the SmartDesign
                Canvas and will not be present in the exported SmartDesign component Tcl
                description.
sd_rename_port -sd_name {smartdesign component name} \
               -current_port_name {port name} \
               -new_port_name {new port name}Arguments
| Parameter | Type | Description | 
|---|---|---|
| sd_name | string | Specifies the name of the SmartDesign component. It is mandatory. | 
| current_port_name | string | Specifies the name of the port to be renamed in the SmartDesign
                                component. It is mandatory.  Note: Only port names
                                    can be renamed, and not port types (scalar ports cannot be
                                    renamed as bus ports and vice versa).  | 
| new_port_name | string | Specifies the new name of the specified port. It is mandatory. | 
| Return Type | Description | 
|---|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|---|
| None | 'P*' is containing the invalid character '*'. | 
| None | Parameter 'new_port_name' has illegal value. | 
| None | Required parameter 'sd_name' is missing. | 
| None | Parameter 'current_port_name' has illegal value. | 
| None | Port 'port_name' doesn't exist. | 
| None | Required parameter 'current_port_name' is missing. | 
| None | Required parameter 'new_port_name' is missing. | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'sd_rename_port -sd_name "sd_name" -current_port_name "current_port_name" -new_port_name "new_port_name"'. | 
| SDCTRL02 | Port name already exists. | 
Supported Families
| Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
Example
The following command renames c1 port name with c2 in "top" design:
sd_rename_port -sd_name {top} -current_port_name {c1} -new_port_name {c2}See Also
- sd_create_scalar_port