Description
This tcl command connects all pins of an instance to new SmartDesign top level ports.
sd_connect_instance_pins_to_ports -sd_name {smartdesign component name} \
                                  -instance_name {instance name}
Arguments
| Parameter | Type | Description | 
|---|
| sd_name | string | Specifies the name of the SmartDesign component. It is mandatory. | 
| instance_name | string | Specifies the instance name for which all the pins must be connected to top level ports. It is mandatory. | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | Parameter 'instance_name' has illegal value. | 
| None | Required parameter 'instance_name' is missing. | 
| None | Parameter 'sd_name' has illegal value. | 
| None | Required parameter 'sd_name' is missing. | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'sd_connect_instance_pins_to_ports -sd_name "sd_name" -instance_name "instance_name"'. | 
Supported Families
            
            | Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
 
        Example
This example connects pins to ports of the instance {CORESPI_C0_0}.
sd_connect_instance_pins_to_ports -sd_name {top} \
                                  -instance_name {CORESPI_C0_0}