Description
This Tcl command sets synthesis attribute to the specified instance of the specified SmartDesign. The attribute is added in the HDL file at the component generation.
sd_set_inst_synth_attr \
        -sd_name {SmartDesign component name} \
        -instance_name {instance name} \
        -attr_name {synthesis attribute name} \
        -attr_value {synthesis attribute value}
Arguments
| Parameter | Type | Description | 
|---|
| sd_name | string | This argument is used to specify the name of the SmartDesign component in which the port synthesis attribute is set. This is a mandatory argument. | 
| instance_name | string | Name of the instance in SmartDesign that synthesis attribute is added to. This is a mandatory argument. | 
| attr_name | string | Synthesis attribute. This is a mandatory argument. | 
| attr_value | string | Value of the attribute. Some attributes do not require values. | 
Synthesis Attributes
            
            The following is the list of attributes and directives available in the Synopsys® FPGA synthesis tool that are supported by SmartDesign. 
            
                        
                            | Name | 
                            Object | 
                            Attribute/Directive | 
                        
                    
                        
                            | syn_insert_buffer | 
                            port, instance | 
                            Attribute | 
                        
                        
                            | syn_keep | 
                            net | 
                            Directive | 
                        
                        
                            | syn_maxfan | 
                            port, net, instance, register | 
                            Attribute | 
                        
                        
                            | syn_no_compile_point | 
                            module/architecture | 
                            Attribute | 
                        
                        
                            | syn_noclockbuf | 
                            port, net, module/architecture | 
                            Attribute | 
                        
                        
                            | syn_noprune | 
                            instance, module/architecture | 
                            Directive | 
                        
                        
                            | syn_preserve | 
                            register, port, module/architecture | 
                            Directive | 
                        
                    
 
        | Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | Instance 'instance_name' does not exist. | 
| None | Parameter 'instance_name' has illegal value. | 
| None | Required parameter 'instance_name' is missing. | 
| None | Parameter 'attr_value' has illegal value. | 
| None | Required parameter 'attr_value' is missing. | 
| None | Parameter 'attr_name' has illegal value. | 
| None | Required parameter 'attr_name' is missing. | 
| None | Parameter 'sd_name' has illegal value. | 
| None | Required parameter 'sd_name' is missing. | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'sd_set_inst_synth_attr -sd_name "sd_name" -attr_name "attr_name" -attr_value "attr_value" -instance_name "instance_name"'. | 
Supported Families
            
            | Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
 
        Example
This example sets "syn_insert_buffer" attribute with "none" value on the "COREABC_C0_0" instance in the "top" design.
sd_set_inst_synth_attr -sd_name {top} -attr_name {syn_insert_buffer} \
                       -attr_value {none} -instance_name {COREABC_C0_0}
See Also
- sd_remove_inst_synth_attr