Description
This tcl command deletes a pin group from an instance in a SmartDesign component.
sd_delete_pin_group -sd_name {smartdesign component name} \
                    -instance_name {instance name} \
                    -group_name {group name}
Arguments
| Parameter | Type | Description | 
|---|
| sd_name | string | Specifies the name of the SmartDesign component. It is mandatory. | 
| instance_name | string | Specifies the name of the instance from which the group pin needs to be deleted. It is mandatory. | 
| group_name | string | Specifies the name of the pin group to be deleted. It is mandatory. | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | Required parameter 'sd_name' is missing. | 
| None | Required parameter 'instance_name' is missing. | 
| None | Required parameter 'group_name' is missing. | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'sd_delete_pin_group -sd_name "sd_name" -group_name "group_name" -instance_name "instance_name"'. | 
| SDCTRL05 | Pin 'group_name' does not exist. | 
Supported Families
            
            | Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
 
        Example
The following example deletes the "MyGroup" group on the "COREAXINTERCONNECT_C0_0" instance in the "TOP" design:
sd_delete_pin_group -sd_name {TOP} \
                    -instance_name {COREAXINTERCONNECT_C0_0} \
                    -group_name {MyGroup}
See Also
- sd_create_pin_group
 - sd_add_pins_to_group
 - sd_rename_pin_group
 - sd_remove_pins_from_group