21.4.29 sd_duplicate_instance
(Ask a Question)Description
This tcl command creates a new instance in a SmartDesign with the same module/component as the original instance.
sd_duplicate_instance 
            -sd_name {smartdesign component name} \
            -instance_name {instance name} \
            [-duplicate_instance_name {duplicate instance name}]Arguments
| Parameter | Type | Description | 
|---|---|---|
sd_name  | string  | Specifies the name of the SmartDesign component. It is mandatory.  | 
instance_name  | string  | Specifies the name of the instance to be duplicated. It is mandatory.  | 
duplicate_instance_name  | string  | Specifies the name of the duplicate instance. It is optional. If value is not specified the default name is provided.  | 
| Return Type | Description | 
|---|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|---|
None  | Parameter 'instance_name' has illegal value.  | 
None  | Required parameter 'instance_name' is missing.  | 
None  | Parameter 'sd_name' has illegal value.  | 
None  | Required parameter 'sd_name' is missing.  | 
None  | Parameter 'param_name' is not defined. Valid command formatting is 'sd_duplicate_instance -sd_name "sd_name" -instance_name "instance_name" [-duplicate_instance_name "duplicate_instance_name"]'.  | 
Supported Families
| Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
Example
This example duplicates "PF_CCC_C0_0" instance.
sd_duplicate_instance -sd_name {top} -instance_name {PF_CCC_C0_0}This example dupicates {PF_CCC_C0_0} instance with {abc_1} name.
sd_duplicate_instance -sd_name {top} \ 
                      -instance_name {PF_CCC_C0_0} \
                      -duplicate_instance_name {abc_1}See Also
sd_disconnect_instance