Description
This Tcl command creates a scalar port in a SmartDesign component.
sd_create_scalar_port -sd_name {smartdesign component name} \
                      -port_name {port name} \
                      -port_direction {IN|OUT|INOUT} 
Arguments
| Parameter | Type | Description | 
|---|
| sd_name | string | Specifies the name of the SmartDesign component. It is mandatory. | 
| port_name | string | Specifies the name of the port added to the SmartDesign component. It is mandatory. | 
| port_direction | string | Specifies the direction of the port added to the SmartDesign component. It is mandatory. | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | Invalid argument value: '' (expecting IN, OUT or INOUT). | 
| None | Parameter 'port_name' has illegal value. | 
| None | Required parameter 'sd_name' is missing. | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'sd_create_scalar_port -sd_name "sd_name" -port_name "port_name" -port_direction "IN | OUT | INOUT"'. | 
Supported Families
            
            | Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
 
        Example
The following tcl command creates "P1" scalar input port in the "main" design:
sd_create_scalar_port -sd_name {main} \
                      -port_name {P1} \
                      -port_direction {IN}