21.4.8 sd_connect_pins_to_constant
(Ask a Question)Description
This tcl command connects SmartDesign top level output ports or input instance pins to constant values.
Important: This
                command will not work on multiple pins in release v2021.1. Support for multiple pins
                will be provided in the next Libero
            release.
sd_connect_pins_to_constant -sd_name {smartdesign component name} \ -pin_names {port or pin names} \ -value {constant value}Arguments
| Parameter | Type | Description | 
|---|---|---|
| sd_name | string | Specifies the name of the SmartDesign component. It is mandatory. | 
| pin_names | string | Specifies the names of the top level output ports or the instance level input pins to be tied to constant values. It is mandatory. | 
| value | string | Specifies the constant value to be assigned to the port/pin. It is mandatory. The acceptable values to this argument are GND/VCC/hexadecimal numbers. | 
| Return Type | Description | 
|---|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|---|
| None | Parameter 'value' has illegal value. | 
| None | Required parameter 'value' is missing. | 
| None | Parameter 'pin_names' has illegal value. | 
| None | Required parameter 'pin_names' is missing. | 
| None | Parameter 'sd_name' has illegal value. | 
| None | Required parameter 'sd_name' is missing. | 
None  | The component 'design_name' doesn't exist. | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'sd_connect_pins_to_constant -sd_name "sd_name" -pin_names "pin_names" -value "value"'. | 
| SDCTRL05 | Pin 'pin_name' does not exist. | 
Supported Families
| Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
Example
This example connects "bypass" pin to "GND".
sd_connect_pins_to_constant -sd_name {top} \ -pin_names {bypass} \ -value {GND}