21.4.13 sd_create_bif_port
(Ask a Question)Description
This Tcl command creates a SmartDesign Bus Interface port of a given type. This command is used to create top level Bus Interface ports in a SmartDesign component to connect to the instance level Bus Interface ports of the same type.
sd_create_bif_port -sd_name {smartdesign component name} \
                   -port_name {port name} \
                   -port_bif_vlnv {vendor:library:name:version} \
                   -port_bif_role {port bif role} \
                   -port_bif_mapping {[bif port name:port name]+}Arguments
| Parameter | Type | Description | 
|---|---|---|
| sd_name | string | Specifies the name of the SmartDesign component. It is mandatory. | 
| port_name | string | Specifies the name of the Bus Interface port to be added in the SmartDesign. It is mandatory. | 
| port_bif_vlnv | string | Specifies the version identifier of the Bus Interface port to be added in the SmartDesign. It is mandatory. | 
| port_bif_role | string | Specifies the role of the Bus Interface port to be added in the SmartDesign. | 
| port_bif_mapping | string | Specifies the mapping between the bus interface formal names and the SmartDesign ports mapped onto that bus interface port. It is mandatory. | 
| Return Type | Description | 
|---|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|---|
None  | Required parameter 'sd_name' is missing.  | 
None  | Parameter 'sd_name' has illegal value.  | 
None  | The component 'design_name' does not exist.  | 
None  | Required parameter 'port_name' is missing.  | 
None  | Parameter 'port_name' has illegal value.  | 
None  | Required parameter 'port_bif_vlnv' is missing.  | 
None  | Parameter 'port_bif_vlnv' has illegal value.  | 
None  | Parameter 'port_bif_role' has illegal value.  | 
None  | Required parameter 'port_bif_role' is missing.  | 
| None | Parameter 'port_bif_mapping' has illegal value.  | 
| None | Required parameter 'port_bif_mapping' is missing.  | 
SDCTRLO2  | Port name 'bif_name' already exist.  | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'sd_create_bif_port -sd_name "sd_name" -port_name "port_name" -port_bif_vlnv "port_bif_vlnv" -port_bif_role "port_bif_role" -port_bif_mapping "[port_bif_mapping]+"'.  | 
Supported Families
| Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
Example
This example creates bif port with "BIF_1" name, "AMBA:AMBA2:APB:r0p0" vendor:library:name:version, {"PADDR:PADDR" \"PENABLE:PENABLE" \ "PWRITE:PWRITE" \ "PRDATA:PRDATA" \ "PWDATA:PWDATA" \ "PREADY:PREADY" } bif mapping and "slave" role:
sd_create_bif_port -sd_name {sd1} \
                   -port_name {BIF_1} \
                   -port_bif_vlnv {AMBA:AMBA2:APB:r0p0} \
                   -port_bif_role {slave} \
                   -port_bif_mapping {"PADDR:PADDR" \                                                                   
                                      "PENABLE:PENABLE" \
                                      "PWRITE:PWRITE" \
                                      "PRDATA:PRDATA" \
                                      "PWDATA:PWDATA" \
                                      "PREADY:PREADY" }See Also
hdl_core_add_bif
hdl_core_assign_bif_signal
sd_create_bif_net