Description
This tcl command allows you to change the presentation view. It takes the SmartDesign name and
                file path as a parameter containing all the presentation data.
-sd_name {SmartDesign_component_name}
-pm_model_file {Presentation_data_path}
Arguments
| Parameter | Type | Description | 
|---|
| sd_name | string | Specifies the name of the SmartDesign on which the presentation will be changed. It is
                                mandatory. | 
| pm_model_file | string | Specifies the file path which contains the presentation data. It is mandatory. | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | Error: {Path} file does not exist. | 
| None | Error: {Path} file does not have read access | 
| None | Required parameter 'sd_name' is missing. | 
| None | The component 'SmartDesign_component_name' does not
                                exist. | 
| None | Required parameter 'pm_model_file' is missing. | 
Supported Families
            
            | Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
 
        Example
The following example changes the presentation view of a SmartDesign.
sd_apply_presentation -sd_name {sd} -pm_model_file {/home/user/sd.pm}