Description
This tcl command creates a group of pins in a SmartDesign component. A pin group is only used to manage the complexity of the SmartDesign canvas. There is no actual netlist functionality related to pin group commands. Pin groups cannot be created for top level ports.
sd_create_pin_group -sd_name {smartdesign component name} \
                    -instance_name {instance name} \
		    [-group_name {group name}] \
		    [-pin_names {pin to be added to the group}]
Arguments
| Parameter | Type | Description | 
|---|
| sd_name | string | Specifies the name of the SmartDesign component. It is mandatory. | 
| instance_name | string | Specifies the name of the instance on which the pin group is added. It is mandatory. | 
| group_name | string | Specifies the name of the pin group. It is optional. If the group name is not specified, the default name will be 'Group'. If the name 'Group' is already taken, then the group name will be 'Group_<index>' (index is auto-incremented). | 
| pin_names | list of strings | Specifies the list of instance pins to be added to the pin group(example below). It is optional. | 
| Return Type | Description | 
|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|
| None | Unconnected input pin "instace_name":"pin_name". | 
| None | Parameter 'param_name' is not defined. Valid command formatting is 'sd_create_pin_group -sd_name "sd_name" [-group_name "group_name"] -instance_name "instance_name" [-pin_names "[pin_names]+"]'. | 
| None | Required parameter 'sd_name' is missing. | 
| None | Required parameter 'instance_name' is missing. | 
Supported Families
            
            | Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
 
        Example
The following example creates a pin group named "MyGroup" on the "COREAXINTERCONNECT_C0_0" instance in the "TOP" design:
sd_create_pin_group -sd_name {TOP} \
                    -instance_name {COREAXINTERCONNECT_C0_0} \
                    -group_name {MyGroup} \
                    -pin_names {ACLK ARESETN}
The following example creates a group of "FORCE_DISP", "DISP_SEL" and "WA_RSTn" pins in a "TOP" design named "MyGroup" on the "CorePCS_C0_0" instance:
sd_create_pin_group -sd_name {TOP} \
                    -group_name {MyGroup} \
                    -instance_name {CorePCS_C0_0} \
                    -pin_names {"FORCE_DISP" "DISP_SEL" "WA_RSTn"}
See Also
- sd_add_pins_to_group
 - sd_delete_pin_group
 - sd_rename_pin_group
 - sd_remove_pins_from_group