21.4.14 sd_create_bus_net
(Ask a Question)Description
This tcl command creates a bus net of a given range in a SmartDesign component. Any net created must be connected to two or more ports/pins using the command “sd_connect_net_to_pins”.
sd_create_bus_net -sd_name {smartdesign component name} \
                  -net_name {net name} \
                  -net_range [left index range:right index range]Arguments
| Parameter | Type | Description | 
|---|---|---|
sd_name  | string  | Specifies the name of the SmartDesign component. It is mandatory.  | 
net_name  | string  | Specifies the name of the net to be added in the SmartDesign component. It is mandatory.  | 
net_range  | string  | Specifies the range of the net added to the SmartDesign component. The range is defined by its left and right rangeindices. It is mandatory.  | 
| Return Type | Description | 
|---|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|---|
None  | Parameter 'net_range' has illegal value.  | 
None  | Required parameter 'net_range' is missing.  | 
None  | Parameter 'net_name' has illegal value.  | 
None  | Required parameter 'net_name' is missing.  | 
None  | Parameter 'sd_name' has illegal value.  | 
None  | Required parameter 'sd_name' is missing.  | 
None  | Parameter 'param_name' is not defined. Valid command formatting is 'sd_create_bus_net -sd_name "sd_name" -net_name "net_name" -net_range "net_range"'.  | 
Supported Families
| Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
Example
This example creates bus net in range [5:0] named "ab1" and connects it to the "RAM64x12_0:R_ADDR" and "a" pins.
This new net is visible in the UI only when it is connected to two or more ports/pins using the command“sd_connect_net_to_pins” as shown below.
sd_create_bus_net -sd_name {top} \
                  -net_name {ab1} \
                  -net_range {[5:0]]}
sd_connect_net_to_pins -sd_name {top} \
                       -net_name {ab1} \
                       -pin_names {a RAM64x12_0:R_ADDR}See Also
sd_connect_net_to_pins
sd_create_bus_port