21.4.25 sd_delete_pin_slices
(Ask a Question)Description
This tcl command deletes SmartDesign top level port slices or instance pin slices.
sd_delete_pin_slices -sd_name {smartdesign component name} \
                     -pin_name {port or pin name} \
                     -pin_slices {port or pin slices}Arguments
| Parameter | Type | Description | 
|---|---|---|
sd_name  | string  | Specifies the name of the SmartDesign component. It is mandatory.  | 
pin_name  | string  | Specifies the name of the bus port or bus pin for which the slices must be deleted. It is mandatory.  | 
pin_slices  | string  | Specifies the ranges of the port and/or pin slices to be deleted. It is mandatory.  | 
| Return Type | Description | 
|---|---|
| None | None | 
Error Codes
| Error Code | Description | 
|---|---|
None  | Parameter 'pin_slices' has illegal value.  | 
None  | Required parameter 'pin_slices' is missing.  | 
None  | Parameter 'pin_name' has illegal value.  | 
None  | Required parameter 'pin_name' is missing.  | 
None  | Parameter 'sd_name' has illegal value.  | 
None  | Required parameter 'sd_name' is missing.  | 
None  | Parameter 'param_name' is not defined. Valid command formatting is 'sd_delete_pin_slices -sd_name "sd_name" -pin_name "pin_name" -pin_slices "[Ranges of pin slices]+"'.  | 
SDCTRL05  | Pin 'pin_name' does not exist. | 
Supported Families
| Supported Families | 
|---|
| PolarFire® | 
| PolarFire SoC | 
| RTG4™ | 
| SmartFusion® 2 | 
| IGLOO® 2 | 
Example
This example deletes {[17:16] [15:1] [0]} slices of "A" pin.
sd_delete_pin_slices -sd_name {top} \
                     -pin_name {A} \
                     -pin_slices {[17:16] [15:1] [0]}See Also
sd_create_pin_slices