16.4.3.1 Sampling Time Requirements
The analog input model of the ADC is illustrated in Figure 16-2.
Time is required to charge the Holding Capacitor (CHOLD) to the input signal level through the source and internal device resistance.
The total acquisition time for the Analog-to-Digital conversion is a function of the Holding Capacitor (CHOLD) charge time. For the ADC module to meet its specified accuracy, the Holding Capacitor (CHOLD) must be allowed to fully charge to the voltage level on the analog input pin. The Signal Source Impedance (RS) and the Interconnect Impedance (RIC) combine to directly affect the time required to charge the CHOLD. The combined impedance (RTOTAL = RS + RIC) must, therefore, be small enough to fully charge the Holding Capacitor within the selected sample time. To charge the CHOLD with 0.5 LSB error, the sampling time should be more than the time defined by the Minimum Sampling Time equation.
For 12-Bit Resolution:
- The CPIN value depends on the device package and is not tested. For QFN or TQFP packages, the typical value is about 4 pF.
- See RIC value in the Electrical Specifications. The typical value is less than 1 kOhm.
- See CHOLD value in the Electrical Specifications. The typical value is about 1 pF.