1.2.5.38 ADP_SetRequest Function
C
void ADP_SetRequest (
uint32_t attributeId,
uint16_t attributeIndex,
uint8_t attributeLength,
const uint8_t *pAttributeValue
);Summary
This primitive sets the value of an attribute in the ADP information base.
Description
The ADP Set Request primitive allows the upper layer to set the value of an attribute in the ADP information base. Result is provided in the corresponding ADP Set Confirm callback.
Parameters
| Param | Description |
|---|---|
| attributeId | The identifier of the ADP IB attribute to read. See ADP_PIB_ATTRIBUTE |
| attributeIndex | The index within the table of the specified IB attribute to read |
| attributeLength | The length of the value of the attribute to set |
| pAttributeValue | Pointer to the value of the attribute to set |
Returns
None.
Example
uint8_t pAttributeValue[64]; pAttributeValue[0] = 44; ADP_SetRequest(ADP_IB_LOW_LQI_VALUE, 0, 1, pAttributeValue); // Wait for Set Confirm
Remarks
None.