1.2.5.25 ADP_PAN_DESCRIPTOR Struct
C
typedef struct
{
/* The 16-bit PAN identifier */
uint16_t panId;
/* The 16 bit short address of a device in this PAN to be used as the LBA
* by the associating device */
uint16_t lbaAddress;
/* The estimated route cost from LBA to the coordinator */
uint16_t rcCoord;
/* The 8-bit link quality of LBA */
uint8_t linkQuality;
/* The media type (PLC or RF) used to communicate with LBA */
uint8_t mediaType;
} ADP_PAN_DESCRIPTOR;Summary
Defines the structure of a PAN Descriptor.
Description
This data type defines the structure of a PAN Descriptor. It used in ADP Discovery Indication to store the parameters of the discovered PAN.
Field description:
- panId. The 16-bit PAN identifier.
- lbaAddress. The 16 bit short address of a device in this PAN to be used as the LBA (LoWPAN Bootstrap Agent) by the associating device.
- rcCoord. The estimated route cost from LBA to the PAN Coordinator.
- linkQuality. The Link Quality measured when receiving frames from the LBA.
- mediaType. The media type (PLC or RF) on which the frame from LBA was received.
Remarks
None.