1.2.5.85 LBP_AdpNetworkJoinRequest Function
C
void LBP_AdpNetworkJoinRequest (
uint16_t panId,
uint16_t lbaAddress,
uint8_t mediaType
);Summary
This primitive allows the upper layer to join an existing network.
Description
The LBP Join Request primitive allows the upper layer to join an existing network.
Result is provided in the corresponding LBP Join Confirm callback.
Parameters
| Param | Description |
|---|---|
| panId | The 16-bit PAN identifier of the network to join |
| lbaAddress | The 16-bit short address of the device acting as a 6LowPAN bootstrap agent (relay) |
| mediaType | The Media Type to use for frame exchange with LBA. Only used in Hybrid Profile. |
Returns
None.
Example
App_DiscoveryIndication(ADP_PAN_DESCRIPTOR *panDescriptor)
{
uint8_t mediaType = MAC_WRP_MEDIA_TYPE_REQ_PLC_BACKUP_RF;
if (panDescriptor-> == MAC_WRP_MEDIA_TYPE_IND_RF)
{
mediaType = MAC_WRP_MEDIA_TYPE_REQ_PLC_BACKUP_PLC;
}
LBP_AdpNetworkJoinRequest(panDescriptor->panId, panDescriptor->panId,
mediaType);
// Wait for Join Confirm
}Remarks
This function is part of the Device LBP Module.