1.2.5.35 ADP_MacGetRequestSync Function
C
void ADP_MacGetRequestSync (
uint32_t attributeId,
uint16_t attributeIndex,
ADP_MAC_GET_CFM_PARAMS* pGetConfirm
);Summary
This primitive gets the value of an attribute from the MAC information base synchronously.
Description
The ADP MAC Get Request primitive allows the upper layer to get the value of an attribute from the MAC information base synchronously. The upper layer cannot access directly the MAC layer while ADP is running. Result is provided directly in one of the function call parameters.
Parameters
| Param | Description |
|---|---|
| attributeId | The identifier of the MAC IB attribute to read. See MAC_WRP_PIB_ATTRIBUTE |
| attributeIndex | The index within the table of the specified IB attribute to read |
| pGetConfirm | Pointer to Get Confirm parameters containinf result and value. See ADP_MAC_GET_CFM_PARAMS |
Returns
None.
Example
ADP_MAC_GET_CFM_PARAMS getConfirm;
ADP_MacGetRequestSync(MAC_WRP_PIB_SHORT_ADDRESS, 0, &getConfirm);
// Check the result
if (getConfirm->status == G3_SUCCESS)
{
// Value is stored in getConfirm->attributeValue
}Remarks
None.