1.2.5.63 ADP_ROUTE_NOT_FOUND_IND_CALLBACK Typedef
C
typedef void (*ADP_ROUTE_NOT_FOUND_IND_CALLBACK)(ADP_ROUTE_NOT_FOUND_IND_PARAMS* pRouteNotFoundInd);
Summary
Pointer to a Route Not Found Indication Event handler function.
Description
This data type defines the required function signature for the ADP Route Not Found Indication event handling callback function. The ADP Route Not Found Indication primitive is used to indicate the upper layer that a route is not available. A client must register a pointer using the event handling function whose function signature (parameter and return value types) matches the types specified by this function pointer in order to receive Route Not Found Indication events back from module.
Parameters
| Param | Description |
|---|---|
| pRouteNotFoundInd | Pointer to structure containing the Broken Route data. See ADP_ROUTE_NOT_FOUND_IND_PARAMS |
Returns
None.
Example
App_RouteNotFoundIndication(ADP_ROUTE_NOT_FOUND_IND_PARAMS *params)
{
// Handle Route Not Found Indication
}Remarks
None.