1.2.5.69 ADP_HOP_DESCRIPTOR Struct
C
typedef struct
{
/* The hop / node address */
uint16_t hopAddress;
/* MetricNotSupported: 1 (the metric type is not supported by the hop) or 0
* (if supported) */
uint8_t mns;
/* LinkCost of the hop */
uint8_t linkCost;
/* Phase Differential on link */
uint8_t phaseDiff;
/* Medium from which request is received */
uint8_t mrx;
/* Medium to which request is transmitted */
uint8_t mtx;
/* Reserved Bits. Read from incoming frame to propagate them correctly. */
uint8_t rsvBits;
} ADP_HOP_DESCRIPTOR;Summary
Defines the structure of a Hop Descriptor.
Description
This data type defines the structure of a Hop Descriptor. It used to describe a hop in a route.
Field description:
- hopAddress. The hop / node address.
- mns. MetricNotSupported: 1 (the metric type is not supported by the hop) or 0 (if supported).
- linkCost. LinkCost of the hop.
- phaseDiff. Phase Differential on link.
- mrx. Medium from which request is received.
- mtx. Medium to which request is transmitted.
- rsvBits. Reserved Bits. Read from incoming frame to propagate them correctly.
Remarks
None.