1.2.5.81 LBP_SET_PARAM_CONFIRM Struct
C
typedef struct
{
/* The identifier of the IB attribute to set */
uint32_t attributeId;
/* The index within the table of the specified IB attribute */
uint16_t attributeIndex;
/* The result of the set request */
LBP_STATUS status;
} LBP_SET_PARAM_CONFIRM;Summary
Defines the parameters for the result of setting a LBP parameter.
Description
The structure contains the the result of setting a LBP parameter.
Field description:
- attributeId. The identifier of the IB attribute to set.
- attributeIndex. The index within the table of the specified IB attribute.
- status. The result of the set request. See LBP_STATUS.
Remarks
None.