1.2.5.71 ADP_PLC_BAND Enum
C
typedef enum
{
/* Success */
G3_SUCCESS = 0x00,
/* Invalid request */
G3_INVALID_REQUEST = 0xA1,
/* Request failed */
G3_FAILED = 0xA2,
/* Invalid IPv6 frame */
G3_INVALID_IPV6_FRAME = 0xA3,
/* Not permited */
G3_NOT_PERMITED = 0xA4,
/* No route to destination */
G3_ROUTE_ERROR = 0xA5,
/* Operation timed out */
G3_TIMEOUT = 0xA6,
/* An attempt to write to a PIB attribute that is in a table failed
* because the specified table index was out of range */
G3_INVALID_INDEX = 0xA7,
/* A parameter in the primitive is either not supported or is out of
* the valid range */
G3_INVALID_PARAMETER = 0xA8,
/* A scan operation failed to find any network beacons */
G3_NO_BEACON = 0xA9,
/* A Set Request was issued with the identifier of an attribute that is read
* only */
G3_READ_ONLY = 0xB0,
/* A Set/Get Request was issued with the identifier of a PIB attribute that
* is not supported */
G3_UNSUPPORTED_ATTRIBUTE = 0xB1,
/* The path discovery has only a part of the path to its desired final
* destination */
G3_INCOMPLETE_PATH = 0xB2,
/* Busy: operation already in progress */
G3_BUSY = 0xB3,
/* Not enough resources */
G3_NO_BUFFERS = 0xB4,
/* Trickle redundancy detected */
G3_TRICKLE_REDUNDANT = 0xB5,
/* Error internal */
G3_ERROR_INTERNAL = 0xFF
} ADP_RESULT;Summary
Identifies the list of errors returned by the ADP.
Description
This enumeration identifies the list of errors returned by the ADP on different operations.
Remarks
None.