1.2.5.80 LBP_SetParamDev Function
C
void LBP_SetParamDev (
uint32_t attributeId,
uint16_t attributeIndex,
uint8_t attributeLen,
const uint8_t *pAttributeValue,
LBP_SET_PARAM_CONFIRM *pSetConfirm
);Summary
Sets the value of a parameter in LBP IB.
Description
This routine allows the upper layer to set the value of a parameter in LBP Information Base.
Parameters
| Param | Description |
|---|---|
| attributeId | Attribute identifier. See LBP_ATTRIBUTE |
| attributeIndex | Index in Table, in case Attribute is a table |
| attributeLen | Length of value to set |
| pAttributeValue | Pointer to value to set |
| pSetConfirm | Pointer to structure containing the set result. See LBP_SET_PARAM_CONFIRM |
Returns
None.
Example
uint8_t psk[16]; LBP_SET_PARAM_CONFIRM setConfirm; LBP_SetParamDev(LBP_IB_PSK, 0, 16, &psk, &setConfirm); if (setConfirm.status == LBP_STATUS_OK) { }
Remarks
This function is part of the Device LBP Module.