1.2.5.39 ADP_SetRequest Function
C
void ADP_SetRequest (
uint32_t attributeId,
uint16_t attributeIndex,
uint8_t attributeLength,
const uint8_t *pAttributeValue,
ADP_SET_CFM_PARAMS* pSetConfirm
);Summary
This primitive sets the value of an attribute in the ADP information base synchronously.
Description
The ADP Set Request primitive allows the upper layer to set the value of an attribute in the ADP information base synchronously. Result is provided directly in one of the function call parameters.
Parameters
| Param | Description |
|---|---|
| attributeId | The identifier of the ADP IB attribute to read. See ADP_PIB_ATTRIBUTE |
| attributeIndex | The index within the table of the specified IB attribute to read |
| attributeLength | The length of the value of the attribute to set |
| pAttributeValue | Pointer to the value of the attribute to set |
| pSetConfirm | Pointer to Set Confirm parameters containing result. See ADP_SET_CFM_PARAMS |
Returns
None.
Example
uint8_t pAttributeValue[64]; ADP_SET_CFM_PARAMS setConfirm; pAttributeValue[0] = 44; ADP_SetRequestSync(ADP_IB_LOW_LQI_VALUE, 0, 1, pAttributeValue, &setConfirm); // Check the result if (setConfirm->status == G3_SUCCESS) { }
Remarks
None.