1.2.5.16 ADP_DataRequest Function
C
void ADP_DataRequest (
uint16_t nsduLength,
const uint8_t *pNsdu,
uintptr_t nsduHandle,
bool discoverRoute,
uint8_t qualityOfService
);Summary
This primitive requests the transfer of a PDU to another device or multiple devices.
Description
The ADP Data Request primitive is used to transfer data to to another device or multiple devices in the G3 Network. Result is provided in the corresponding ADP Data Confirm callback.
Parameters
| Param | Description |
|---|---|
| nsduLength | The size of the NSDU, in bytes; Up to 1280 |
| pNsdu | Pointer to NSDU to send; has to be a valid IPv6 packet |
| nsduHandle | The handle of the NSDU to transmit. This parameter is used to identify in the ADP Data Confirm primitive which request it is concerned with. It can be randomly chosen by the application layer. |
| discoverRoute | If true, a route discovery procedure will be performed prior to sending the frame if a route to the destination is not available in the routing table. If false, no route discovery is performed. |
| qualityOfService | The requested quality of service (QoS) of the frame to send. Allowed values are 0 (normal priority) and 1 (high priority). |
Returns
None.
Example
uint8_t nsdu[1280]; uint16_t nsduLength; // ... // Fill NSDU // ... ADP_DataRequest(nsduLength, nsdu, 0, true, 0); // Wait for Data Confirm
Remarks
None.