1.2.5.21 ADP_DATA_IND_PARAMS Struct
C
typedef struct
{
/* The received NSDU */
const uint8_t* pNsdu;
/* The size of the NSDU, in bytes; Up to 1280 bytes */
uint16_t nsduLength;
/* The value of the link quality during reception of the frame */
uint8_t linkQualityIndicator;
} ADP_DATA_IND_PARAMS;Summary
Defines the Parameters for the ADP Data Indication event handler function.
Description
The structure contains the fields reported by the ADP Data Indication event handler function.
Field description:
- pNsdu. Pointer to the received NSDU.
- nsduLength. The size of the NSDU, in bytes; Up to 1280 bytes.
- linkQualityIndicator. The value of the measured link quality during reception of the frame.
Remarks
None.