1.2.5.54 ADP_PATH_DISCOVERY_CFM_CALLBACK Typedef
C
typedef void (*ADP_PATH_DISCOVERY_CFM_CALLBACK)(ADP_PATH_DISCOVERY_CFM_PARAMS* pPathDiscoveryCfm);
Summary
Pointer to a Path Discovery Confirm Event handler function.
Description
This data type defines the required function signature for the ADP Path Discovery Confirm event handling callback function. The ADP Path Discovery Confirm primitive allows the upper layer to be notified of the completion of an ADP Path Discovery Request. A client must register a pointer using the event handling function whose function signature (parameter and return value types) matches the types specified by this function pointer in order to receive Path Discovery Confirm events back from module.
Parameters
| Param | Description |
|---|---|
| pPathDiscoveryCfm | Pointer to structure containing parameters related to Confirm. See ADP_PATH_DISCOVERY_CFM_PARAMS |
Returns
None.
Example
App_PathDiscoveryConfirm(ADP_LBP_CFM_PARAMS *params)
{
// Check result
if (params->status == G3_SUCCESS)
{
}
}Remarks
None.