1.2.5.20 ADP_DATA_IND_CALLBACK Typedef
C
typedef void (*ADP_DATA_IND_CALLBACK)(ADP_DATA_IND_PARAMS* pDataInd);
Summary
Pointer to a Data Indication Event handler function.
Description
This data type defines the required function signature for the ADP Data Indication event handling callback function. The ADP Data Indication primitive is used to transfer received data from the adaptation sublayer to the upper layer. A client must register a pointer using the event handling function whose function signature (parameter and return value types) matches the types specified by this function pointer in order to receive Data Indication events back from module.
Parameters
| Param | Description |
|---|---|
| pDataInd | Pointer to structure containing parameters related to Indication. See ADP_DATA_IND_PARAMS |
Returns
None.
Example
App_DataIndication(ADP_DATA_IND_PARAMS *params)
{
// Check Link Quality
if (params->linkQualityIndicator > 40)
{
// Check data content in params->pNsdu
}
}Remarks
None.