2.49.61 GPIO_POLARITY Enum
C
The GPIO_POLARITY vary based on device family. Refer to the generated header file for the actual values.
Summary
This enum is used to to specify the pin polarity in the GPIO_PinPolarityConfig API
Description
This enum is used to to specify the pin polarity in the GPIO_PinPolarityConfig API
Remarks
None