2.49.64 GPIO_PWRGATE Enum

C

The GPIO_PWRGATE vary based on device family. Refer to the generated header file for the actual values.

Summary

This enum is used to to specify the power well for the pin in the GPIO_PinPwrGateConfig API

Description

This enum is used to to specify the power well for the pin in the GPIO_PinPwrGateConfig API

Remarks

None