2.49.53 GPIO_INP_READ Enum
C
The GPIO_INP_READ vary based on device family. Refer to the generated header file for the actual values.
Summary
This enum is used to enable or disable input for a pin using the GPIO_PinInputConfig API
Description
This enum is used to enable or disable input for a pin using the GPIO_PinInputConfig API
Remarks
None