2.49.37 GPIO_PinPwrGateConfig Function
C
void GPIO_PinPwrGateConfig(GPIO_PIN pin, GPIO_PWRGATE pwrGate)
Summary
Configures the power well to use for the given GPIO pin
Description
This API lets the application configure the power well for the given GPIO pin
Precondition
None
Parameters
Param | Description |
---|---|
pin | One of the values from the enum GPIO_PIN |
pwrGate | One of the values from the enum GPIO_PWRGATE |
Returns
None
Example
GPIO_PinPwrGateConfig(GPIO_PIN_GPIO012, GPIO_PWR_VCC);
Remarks
None