2.49.62 GPIO_PROPERTY Enum

C

The GPIO_PROPERTY vary based on device family. Refer to the generated header file for the actual values.

Summary

This enum is used to to specify the property of the pin to configure in the GPIO_PropertySet API

Description

This enum is used to to specify the property of the pin to configure in the GPIO_PropertySet API

Remarks

None