2.49.19 GPIO_PinDirConfig Function
C
void GPIO_PinDirConfig(GPIO_PIN pin, GPIO_DIR dir)
Summary
Sets the direction of the given GPIO Pin.
Description
Based on the GPIO_DIR enum value, sets the direction of the given GPIO_PIN
Precondition
None.
Parameters
Param | Description |
---|---|
pin | One of the GPIO pins from the enum GPIO_PIN |
dir | One of the values from the enum GPIO_DIR |
Returns
None
Example
// Set the direction of GPIO_PIN_GPIO012 to output
GPIO_PinDirConfig(GPIO_PIN_GPIO012, GPIO_DIR_OUTPUT);
Remarks
None