2.49.57 GPIO_DIR Enum

C

The GPIO_DIR vary based on device family. Refer to the generated header file for the actual values.

Summary

This enum is used to to specify the GPIO pin direction in the GPIO_PinDirConfig API

Description

This enum is used to to specify the GPIO pin direction in the GPIO_PinDirConfig API

Remarks

None