2.49.59 GPIO_FUNCTION Enum
C
The GPIO_FUNCTION vary based on device family. Refer to the generated header file for the actual values.
Summary
This enum is used to to specify the GPIO pin function to configure a pin to using the GPIO_PinMUXConfig API
Description
This enum is used to to specify the GPIO pin function to configure a pin to using the GPIO_PinMUXConfig API
Remarks
None