2.49.47 GPIO_PinMUXConfig Function
C
void GPIO_PinMUXConfig(GPIO_PIN pin, GPIO_FUNCTION function)
Summary
Configures the signal function on the given pin
Description
This API lets the application select the signal function on the given pin
Precondition
None
Parameters
Param | Description |
---|---|
pin | One of the values from the enum GPIO_PIN |
function | One of the values from the enum GPIO_FUNCTION |
Returns
None
Example
GPIO_PinMUXConfig(GPIO_PIN_GPIO012, GPIO_FUNCTION_GPIO);
Remarks
None