2.49.58 GPIO_DRV Enum
C
The GPIO_DRV vary based on device family. Refer to the generated header file for the actual values.
Summary
This enum is used to to specify the pin drive strength in the GPIO_DrvStrConfig API
Description
This enum is used to to specify the pin drive strength in the GPIO_DrvStrConfig API
Remarks
None