2.58.1 LCDCx_AddToQueueEnable Function
C
// x - Instance of the LCDC peripheral
void LCDCx_AddToQueueEnable(LCDCx_LAYER_ID layer)
Summary
Indicates that a valid descriptor has been written to memory
Description
Indicates that a valid descriptor has been written to memory, its memory location should be written to the DMA head pointer. The A2QSR status bit is set to one, and it is reset by hardware as soon as the descriptor pointed to by the DMA head pointer is added to the list.
Precondition
None.
Parameters
Param | Description |
---|---|
layer | the target layer |
Returns
None