3.1.6 Meter Type Settings Register

This register defines the service type settings and type of meter voltage and current sensors.
Name: METER_TYPE
Property: Read-Write

Bit 3130292827262524 
 Dto4WY_TRANSFORM MISSING_PHASE[1:0]SERVICE_TYPE[3:0] 
Access R/WR/WR/WR/WR/WR/WR/W 
Reset 0000000 
Bit 2322212019181716 
          
Access  
Reset  
Bit 15141312111098 
   SENSOR_TYPE_I_N[1:0]SENSOR_TYPE_V_C[1:0]SENSOR_TYPE_I_C[1:0] 
Access R/WR/WR/WR/WR/WR/W 
Reset 000000 
Bit 76543210 
 SENSOR_TYPE_V_B[1:0]SENSOR_TYPE_I_B[1:0]SENSOR_TYPE_V_A[1:0]SENSOR_TYPE_I_A[1:0] 
Access R/WR/WR/WR/WR/WR/WR/WR/W 
Reset 00000000 

Bit 31 – Dto4WY_TRANSFORM

For use with: 4-Wire and 3-Wire DELTA meters only. Phase voltages (and currents, where applicable) are transformed into an equivalent 4-wire Wye service for metering using alternate equations.
ValueNameDescription
0x0 DISABLED Phase voltages remain in native service (no transformation).
0x1 ENABLED Phase voltages transformed into an equivalent 4-wire Wye service. Transformation may lose accuracy in non-Blondel/unbalanced situations. Meter vector transformation is useful in some applications and possible, transforming 3-Phase Delta meters into an equivalent 3-Phase 4WY. However, it is useful only for balanced voltage situations.

Bits 29:28 – MISSING_PHASE[1:0]  Missing phase voltage select

For use with Poly-phase 4-wire Wye 2-1/2 element meters only.
ValueDescription
0x0 Generate missing phase voltage for Phase_A: V_A = -(V_B + V_C).
0x1 Generate missing phase voltage for Phase_B: V_B = -(V_A + V_C).
0x2 Generate missing phase voltage for Phase_C: V_C = -(V_A + V_B).

Bits 27:24 – SERVICE_TYPE[3:0]  Electrical Service Type

The service type determines what meter form is being implemented and how the Metrology DSP core interprets and processes the ADC values. Refer to the Annex – Meter Forms for additional information.
ValueNameDescription
0x0 3P4WY_3E_3V3I Three-phase 4-wire Wye (3-element)
0x1 3P4WD_3E_3V3I Three-phase 4-wire Delta (3-element).
0x2 3P3P4WY_2p5E_2V3I Three-phase 4-wire Wye (2-½ element)
0x3 3P4WD_2E_3V2I Three-phase 4-wire Delta (2-element)
0x4 3P3WD_2E_2V2I Three-phase 3-wire) Delta (2-element)
0x5 2P3W_2E_2V2I Two-phase 3-wire Network (2 element)
0x6 1P3W_1p5E_1V2I Single-phase 3-wire (1-½ element)
0x7 1P2W_1E_1V1I Single-phase 2-wire (1 element)
0x8 1P3W_1E_2V1I Single-phase 3-wire (1 element)

Bits 13:12 – SENSOR_TYPE_I_N[1:0] Current Sensor Type on N Phase

Selects the types of current and voltage sensor used. Read the following table for additional information.

Bits 11:10 – SENSOR_TYPE_V_C[1:0] Voltage Sensor Type on C Phase

Selects the types of current and voltage sensor used. For each channel selected as using a Rogowski sensor, the Metrology DSP implements a digital integrator filter to normalize the effects of the sensor’s di/dt behavior.
ValueNameDescription
0x0 CURRENT TRANSFORMER —
0x1 RESISTIVE SHUNT May only be used with phase-to-neutral voltage measurement applications.
0x2 ROGOWSKI COIL (CRC) CURRENT SENSOR A digital integrator function is added to the DSP of all current channels selected as using Rogowski Coils. When SENSOR_TYPE_I_x = 2, an additional phase correction is internally added to each channel with a Rogowski sensor in the amount of -0.3704º (@ 60 Hz) to correct for a linear phase response introduced by the digital integrator filter. This is taken into account during the internal calculation of actual phase-correction filter coefficients, when a new set of phase calibration settings are loaded, and must not be added by the user in the phase-correction entries. When SENSOR_TYPE_I_x is set to other values, it takes no effect.
0x3 RESISTIVE DIVIDER (VRD) VOLTAGE SENSOR Normally, this is the typical option selected for voltage sensors.

Bits 9:8 – SENSOR_TYPE_I_C[1:0] Current Sensor Type on C Phase

Selects the types of current and voltage sensor used. Read the previous table for additional information.

Bits 7:6 – SENSOR_TYPE_V_B[1:0] Voltage Sensor Type on B Phase

Selects the types of current and voltage sensor used. Read the previous table for additional information.

Bits 5:4 – SENSOR_TYPE_I_B[1:0] Current Sensor Type on B Phase

Selects the types of current and voltage sensor used. Read the previous table for additional information.

Bits 3:2 – SENSOR_TYPE_V_A[1:0] Voltage Sensor Type on A Phase

Selects the types of current and voltage sensor used. Read the previous table for additional information.

Bits 1:0 – SENSOR_TYPE_I_A[1:0] Current Sensor Type on A Phase

Selects the types of current and voltage sensor used. Read the previous table for additional information.