5.34.98 Arguments
-file name
Specifies the name of the file to which you want to associate your stimulus files.
-mode value
Specifies whether you are creating a new stimulus association, adding, or removing; possible values are:
Value | Description |
new | Creates a new stimulus file association |
add | Adds a stimulus file to an existing association |
remove | Removes an stimulus file association |
-module value
Sets the module, where value is the name of the module.
-tool value
Identifies the intended use for the file, possible values are:
Value | Description |
synthesis | File to be used for synthesis |
simulation | File to be used for simulation |
-use_default value
Uses the default values for synthesis or simulation; possible values are:
Value | Description |
TRUE | Uses default values for synthesis or simulation. |
FALSE | Uses user-defined values for synthesis or simulation |