5.34.110 About Designer Tcl commands
A Tcl (Tool Command Language) file contains scripts for simple or complex tasks. You can run scripts from either the Windows or UNIX command line or store and run a series of Tcl commands in a “.tcl” batch file. You can also run scripts from within Designer.
Designer supports the following Tcl scripting commands. Tcl commands are case sensitive. However, their arguments are not.
| Command | Action |
| add_probe | Adds a probe to an internal net in your design, using the original name from the optimized netlist in your design. Also, this command must be used in conjunction with the generate_probes command to generate a probed ADB file (see example below). |
| all_inputs | Returns an object representing all input and inout pins in the current design. |
| all_outputs | Returns an object representing all output and inout pins in the current design. |
| all_registers | Returns an object representing register pins or cells in the current scenario based on the given parameters. |
| are_all_source_files_current | Audits all source files and determines whether or not they are out of date/imported into the workspace. |
| backannotate | Extracts timing delays from your post layout data. |
| check_timing_constraints | Checks all timing constraints in the current timing scenario for validity. |
| clone_scenario | Creates a new timing scenario by duplicating an existing one. |
| close_design | Closes the current design. |
| compile | Performs design rule check and optimizes the input netlist before translating the source code into machine code. |
| create_clock | Creates a clock constraint on the specified ports/pins, or a virtual clock if no source is specified. |
| create_generated_clock | Creates an internally generated clock constraint on the ports/pins and defines its characteristics. |
| create_scenario | Creates a new timing scenario with the specified name. |
| delete_probe | Deletes a probe on nets in a probed ADB file. |
| delete_scenario | Deletes the specified timing scenario. |
| export | Converts a file from its current format into the specified file format, usually for use in another program. |
| extended_run_shell | Runs multiple iterations of layout through Designer. |
| generate_probes | Executes the probing and creates a new ADB file. This command is used in conjunction with the add_probe Tcl command (see example below). |
| get_cells | Returns an object representing the cells (instances) that match those specified in the pattern argument. |
| get_clocks | Returns an object representing the clock(s) that match those specified in the pattern argument in the current timing scenario. |
| get_current_scenario | Returns the name of the current timing scenario. |
| get_defvar | Returns the value of the Designer internal variable you specify. |
| get_design_filename | Returns the fully qualified path of the specified design file. |
| get_design_info | Returns detailed information about your design, depending on which arguments you specify. |
| get_nets | Returns an object representing the nets that match those specified in the pattern argument. |
| get_out_of_date_files | Audits all files returns a list of filenames that are out of date. |
| get_pins | Returns an object representing the pin(s) that match those specified in the pattern argument. |
| get_ports | Returns an object representing the port(s) that match those specified in the pattern argument. |
| import_aux | Imports the specified file as an auxiliary file, which are not audited and do not require you to re-compile the design. |
| import_source | Imports the specified file as a source file, which include your netlist and design constraints. |
| ioadvisor_apply_suggestion | Applies the suggestions for the selected attribute to the selected I/O(s). |
| ioadvisor_commit | Saves all changes in the I/O Advisor. |
| ioadvisor_restore | Restores the I/O Advisor to the initial state. |
| ioadvisor_restore_initial_value | Sets the current value for the selected attribute and I/Os to the initial value. |
| ioadvisor_set_outdrive | Sets the outdrive for the selected I/Os. |
| ioadvisor_set_outputload | Sets the output load for the selected I/Os. |
| ioadvisor_set_slew | Sets the slew for the selected I/Os. |
| is_design_loaded | Returns True if the design is loaded into Designer; otherwise, returns False. |
| is_design_modified | Returns True if the design has been modified since it was last compiled; otherwise, returns False. |
| is_design_state_complete | Returns True if the specified design state is complete (for example, you can inquire as to whether a die and package has been selected for the design); otherwise, returns False. |
| is_source_file_current | Audits the source file and determines whether or not the file is out of date / imported into the workspace. |
| layout | Place-and-route your design. |
| layout (advanced options for the SX family) | Sets advanced place-and-route features for SX family designs. |
| layout - Axcelerator | Sets advanced place-and-route features for Axcelerator family designs. |
| list_clocks | Returns details about all of the clock constraints in the current timing constraint scenario. |
| list_clock_latencies | Returns details about all of the clock latencies in the current timing constraint scenario. |
| list_clock_uncertainties | Returns the list of clock-to-clock uncertainty constraints for the current scenario. |
| list_disable_timings | Returns the list of disable timing constraints for the current scenario. |
| list_false_paths | Returns details about all of the false paths in the current timing constraint scenario. |
| list_generated_clocks | Returns details about all of the generated clock constraints in the current timing constraint scenario. |
| list_input_delays | Returns details about all of the input delay constraints in the current timing constraint scenario. |
| list_max_delays | Returns details about all of the maximum delay constraints in the current timing constraint scenario. |
| list_min_delays | Returns details about all of the minimum delay constraints in the current timing constraint scenario. |
| list_multicycle_paths | Returns details about all of the multicycle paths in the current timing constraint scenario. |
| list_objects | Returns a list of names of the objects in the specified list. |
| list_output_delays | Returns details about all of the output delay constraints in the current timing constraint scenario. |
| list_scenarios | Returns a list of names of all of the available timing scenarios. |
| new_design | Creates a new design (.adb) file in a specific location for a particular design family such as Axcelerator or ProASIC3. |
| open_design | Opens an existing design in the Designer software. |
| pin_assign | Assigns the named pin to the specified port but does not lock its assignment. |
| pin_commit | Saves the pin assignments to the design (.adb) file. |
| pin_fix | Locks the pin assignment for the specified port, so the pin cannot be moved during place-and-route. |
| pin_fix_all | Locks all the assigned pins on the device so they cannot be moved during place-and-route. |
| pin_unassign | Unassigns a specific pin from a specific port. The unassigned pin location is then available for other ports. |
| pin_unassign_all | Unassigns all pins from a specific port. |
| pin_unfix | Unlocks the specified pin from its port.. |
| layout (advanced options for ProASIC | Sets advanced place-and-route features for ProASIC family designs. |
| remove_clock | Removes the specified clock constraint from the current timing scenario. |
| remove_clock_latency | Removes a clock source latency from the specified clock and from all edges of the clock. |
| remove_clock_uncertainty | Removes a clock-to-clock uncertainty from the current timing scenario by specifying either its exact arguments or its ID. |
| remove_disable_timing | Removes a disable timing constraint by specifying its arguments, or its ID. |
| remove_false_path | Removes a false path from the current timing scenario by specifying either its exact arguments or its ID. |
| remove_generated_clock | Removes the specified generated clock constraint from the current scenario. |
| remove_input_delay | Removes an input delay a clock on a port by specifying both the clocks and port names or the ID of the input_delay constraint to remove. |
| remove_max_delay | Removes a maximum delay constraint in the current timing scenario by specifying either its exact arguments or its ID. |
| remove_min_delay | Removes a minimum delay constraint in the current timing scenario by specifying either its exact arguments or its ID. |
| remove_multicycle_path | Removes a multicycle path constraint in the current timing scenario by specifying either its exact arguments or its ID. |
| remove_output_delay | Removes an ouput delay by specifying both the clocks and port names or the ID of the output_delay constraint to remove. |
| rename_scenario | Renames the specified timing scenario with the new name provided. |
| report | Generates the type of report you specify: Status, Timing, Timer Violations, Flip-flop, Power, Pin, or I/O Bank. |
| report (Activity and Hazards Power Report) | Reads a VCD file and reports transitions and hazards for each clock cycle of the VCD file. |
| report (Bottleneck) using SmartTime | Creates a bottleneck report. |
| report (Cycle Accurate Power Report) | Reports a power waveform with one power value per clock period or half-period instead of an average power for the whole simulation. |
| Report (Data History) | Reports new features and enhancements, bug fixes and known issues for the current release that may impact the power consumption of the design. |
| report (Datasheet) using SmartTime | Creates a datasheet report. |
| Report (Power) | Creates a Power report, which enables you to determine if you have any power consumption problems in your design. |
| Report (Power Scenario) | Creates a scenario power report, which enables you to enter a duration for a sequence of previously defined power modes and calculate the average power consumption and the excepted battery life for this sequence. |
| report (Timing) using SmartTime | Creates a timing report. |
| report (Timing violations) using SmartTime | Creates a timing violations report. |
| set_clock_latency | Defines the delay between an external clock source and the definition pin of a clock within SmartTime. |
| set_clock_uncertainty | Specifies a clock-to-clock uncertainty and returns the ID of the created constraint if the command succeeded. |
| set_current_scenario | Specifies the timing scenario for the Timing Analyzer to use. |
| save_design | Writes the design to the specified filename. |
| set_defvar | Sets the value of the Designer internal variable you specify >. |
| set_design | Specifies the design name, family and path in which Designer will process the design. |
| set_device | Specifies the type of device and its parameters. |
| set_disable_timing | Disables timing a.rcs within a cell and returns the ID of the created constraint. |
| set_false_path | Identifies paths that are considered false and excluded from the timing analysis in the current timing scenario. |
| set_input_delay | Creates an input delay on a port list by defining the arrival time of an input relative to a clock in the current scenario. |
| set_max_delay | Specifies the maximum delay for the timing paths in the current scenario. |
| set_min_delay | Specifies the minimum delay for the timing paths in the current scenario. |
| set_multicycle_path | Defines a path that takes multiple clock cycles in the current scenario. |
| set_output_delay | Defines the output delay of an output relative to a clock in the current scenario. |
| smartpower_add_new_custom_mode | Creates a new custom mode. |
| smartpower_add_new_scenario | Creates a new scenario. |
| smartpower_add_pin_in_domain | Adds a pin to either a Clock or Set domain. |
| smartpower_change_clock_statistics | Changes the default frequencies and probabilities for a specific domain. |
| smartpower_change_setofpin_statistics | Changes the default frequencies and probabilities for a specific set. |
| smartpower_commit | Saves the changes made in SmartPower to the design file (.adb) in Designer. |
| smartpower_create_domain | Creates a new clock or set domain. |
| smartpower_edit_custom_mode | Edits a custom mode. |
| smartpower_edit_scenario | Edits a scenario. |
| smartpower_initialize_clock_with_constraints | Initializes the clock frequency and the data frequency of a single clock domain with a specified clock name and the initialization options. |
| smartpower_init_do | Initializes the frequencies and probabilities for clocks, registers, set/reset nets, primary inputs, combinational outputs, enables and other sets of pins, and selects a mode for initialization. |
| smartpower_init_set_clocks_options | Initializes the clock frequency of all clock domains. |
| smartpower_init_set_combinational_options | Initializes the frequency and probability of all combinational outputs. |
| smartpower_init_set_enables_options | Initializes the clock frequency of all enable clocks with the initialization options. |
| smartpower_init_set_othersets_options | Initializes the frequency and probability of all other sets. |
| smartpower_init_set_primaryinputs_options | Initializes the frequency and probability of all primary inputs. |
| smartpower_init_set_registers_options | Initializes the frequency and probability of all register outputs. |
| smartpower_init_set_set_reset_options | Initializes the frequency and probability of all set/reset nets. |
| smartpower_init_setofpins_values | Initializes the frequency and probability of all sets of pins. |
| smartpower_remove_all_annotations | Removes all initialization annotations for the specified mode. |
| smartpower_remove_custom_mode | Removes a custom mode. |
| smartpower_remove_domain | Removes an existing domain. |
| smartpower_remove_file | Removes a VCD file from the specified mode. |
| smartpower_remove_pin_enable_rate | This command is obsolete and it is replaced by smartpower_remove_pin_probability |
| smartpower_remove_pin_frequency | Removes the frequency of an existing pin. |
| smartpower_remove_pin_of_domain | Removes a clock pin or a data pin from a Clock or Set domain, respectively. |
| smartpower_remove_pin_probability | Enables you to annotate the probability of a pin driving an enable pin. |
| smartpower_remove_scenario | Removes a scenario from the current design. |
| smartpower_remove_vcd | Removes an existing VCD file from a mode or entire design. |
| smartpower_restore | Restores previously committed constraints. |
| smartpower_set_battery_capacity | Sets the battery capacity. |
| smartpower_set_cooling | Sets the cooling style to one of the predefined types, or a custom value. |
| smartpower_set_mode_for_analysis | Sets the mode for cycle-accurate power analysis. |
| smartpower_set_operating_condition | Sets the operating conditions used in SmartPower to best, typical, or worst case. |
| smartpower_set_pin_enable_rate | This command is obsolete and is replaced by smartpower_set_pin_probability. |
| smartpower_set_pin_frequency | Sets the frequency of an existing pin. |
| smartpower_set_pin_probability | Enables you to annotate the probability of a pin driving an enable pin. |
| smartpower_set_preferences | Sets SmartPower preferences such as power unit, frequency unit, operating mode, operating conditions, and toggle. |
| smartpower_set_scenario_for_analysis | Sets the scenario for cycle-accurate power analysis. |
| smartpower_set_temperature_opcond | Sets the temperature in the operating conditions used in SmartPower. |
| smartpower_set_thermalmode | Sets the mode of computing junction temperature. |
| smartpower_set_voltage_opcond | Sets the voltage in the operating conditions used in SmartPower. |
| smartpower_temperature_opcond_set_design_wide | Sets the temperature for SmartPower design-wide operating conditions. |
| smartpower_temperature_opcond_set_mode_specific | Sets the temperature for SmartPower mode-specific operating conditions. |
| smartpower_voltage_opcond_set_design_wide | Sets the voltage settings for SmartPower design-wide operating conditions. |
| smartpower_voltage_opcond_set_mode_specific | Sets the voltage settings for SmartPower mode-specific use operating conditions. |
| st_create_set | Creates a set of paths to be analyzed. |
| st_commit | Saves the changes made in SmartTime to the design (.adb) file. |
| st_edit_set | Modifies the paths in a user set. |
| st_expand_path | Displays expanded path information (path details) for paths. |
| st_list_paths | Displays the list of paths in the same tabular format shown in SmartTime. |
| st_remove_set | Deletes a user set from the design. |
| st_restore | Restores constraints previously committed in SmartTime. |
| st_set_options | Sets options for timing analysis. |
| timer_add_clock_exception | Adds an exception to or from a pin with respect to a specified clock. |
| timer_add_pass | Adds the pin to the list of pins for which the path must be shown passing through in the timer. |
| timer_add_stop | Adds the specified pin to the list of pins through which the paths will not be displayed in the timer. |
| timer_commit | Saves the changes made to constraints in Timer into the Designer database. |
| timer_get_path | Displays the Timer path information in the Log window. |
| timer_get_clock_actuals | Displays the actual clock frequency in the Log window. |
| timer_get_clock_constraints | Displays the clock constraints (period/frequency and dutycycle) in the Log window. |
| timer_get_maxdelay | Displays the maximum delay constraint between two pins of a path in the Log window.timer_get_path_constraintsDisplays the path constraints set for maxdelay in the Timer in the Log window. |
| timer_remove_clock_exception | Removes the previously set clock constraint. |
| timer_remove_pass | Removes the previously entered path pass constraint. |
| timer_remove_stop | Removes the path stop constraint on the specified pin.timer_restoreRestores previously committed constraints.timer_setenv_clock_freqSets a required clock frequency, in MHz, for the specified clock. |
| timer_setenv_clock_period | Sets the clock period constraint for the specified clock. |
| timer_set_maxdelay | Adds a maximum delay constraint for the path. |
| timer_remove_all_constraints | Removes all the timing constraints previously entered in the Designer system. |