5.34.93 Arguments

-file name

Specifies the name of the file to which you want to associate your stimulus files.

-mode value

Specifies whether you are creating a new stimulus association, adding, or removing; possible values are:

Value

Description

new

Creates a new stimulus file association

Value

Description

add

Adds a stimulus file to an existing association

remove

Removes an stimulus file association

-designer_view name

Sets the name of the Designer View in which you wish to add the constraint file, where name is the name of the view (such as impl1).

-module value

Sets the module, where value is the name of the module.

-tool value

Identifies the intended use for the file, possible values are:

Value

Description

synthesis

File to be used for synthesis

designer

File to be used in Designer

phsynth

File to be used in physical synthesis