21.8.3.2 Bottleneck Description
This section displays a graphic representation of the bottleneck analysis and lists the core of the bottleneck information for the bar selected in the chart above. If no bar is selected, the grid lists all bottleneck information.
Click the controls on the right to zoom in or out the contents in the chart. Right-click the
chart to export the chart or to copy the chart to the clipboard. The list is divided into two columns:
- Instance name: refers to the output pin name of the instance. Click the pin name to select the cell and the corresponding instance is selected in MultiView Navigator (MVN).
- Bottleneck cost: displays the pin's cost given the chosen cost type. Pin names are listed in decreasing order of their cost type.