3.4.4.3 DDR3PHY PHY General Status Register

Name: DDR3PHY_PGSR
Offset: 0x0C
Reset: 0x00000000
Property: Read-only

Bit 3130292827262524 
          
Access  
Reset  
Bit 2322212019181716 
          
Access  
Reset  
Bit 15141312111098 
       RVEIRRRVERR 
Access RR 
Reset 00 
Bit 76543210 
 DFTERRDTIERRDTERRDTDONEDIDONEZCDONEDLDONEIDONE 
Access RRRRRRRR 
Reset 00000000 

Bit 9 – RVEIRR Read Valid Training Intermittent Error

If set, indicates that there was an intermittent error during read valid training, such as a pass followed by a fail then followed by another pass.

Bit 8 – RVERR Read Valid Training Error

If set, indicates that a valid read valid placement could not be found during read valid training.

Bit 7 – DFTERR DDR_DQS Drift Error

If set, indicates that at least one of the read data strobes has drifted by more than or equal to the drift limit set in DDR3PHY_PGCR.

Bit 6 – DTIERR DDR_DQS Gate Training Intermittent Error

If set, indicates that there was an intermittent error during DDR_DQS gate training, such as a pass followed by a fail then followed by another pass.

Bit 5 – DTERR DDR_DQS GateTraining Error

If set, indicates that a valid DDR_DQS gating window could not be found during DDR_DQS gate training.

Bit 4 – DTDONE Data Training Done

If set, indicates that the PHY has finished doing data training.

Bit 3 – DIDONE DRAM Initialization Done

If set, indicates that DRAM initialization has completed.

Bit 2 – ZCDONE Impedance Calibration Done

If set, indicates that impedance calibration has completed.

Bit 1 – DLDONE DLL Lock Done

If set, indicates that DLL locking has completed.

Bit 0 – IDONE Initialization Done

If set, indicates that the DDR system initialization has completed. This bit is set after all the selected initialization routines in DDR3PHY_PIR have completed.