3.6.2.4.2 LATENCY_REDUCTION
(Ask a Question)The LATENCY_REDUCTION settings control the SmartHLS's expression balancing optimization, of which the objective is to reduce the circuit latency. Below are the related settings:
Parameter Name | Default Value | Description |
---|---|---|
LATENCY_REDUCTION | 1 | The main switch that enables or disables expression balancing. Setting to 0 disables all expression balancing optimizations. |
LATENCY_REDUCTION_ALLOW_FP_REORDERING | 0 | By default, expression balancing does not re-order floating-point operations to prevent loss of precisions. Setting to 1 allows to re-order floating-point operations if the circuit latency can be reduced. |
LATENCY_REDUCTION_REDUCE_FP_CONVERSIONS | 0 | Setting to 1 will allow SmartHLS™ to cancel out back-and-forth conversion between floating-point and integer, with potential variations in numerical values. For example, the following conversions can be cancelled when this setting is 1.
|
LATENCY_REDUCTION_BALANCE_MULTI_USE_NODE | 0 | By default expression balancing does not optimize the intermediate operations that have multiple uses, to avoid potential increase of resource usage. Setting to 1 allows to re-order intermediate operations that have multiple uses and more latency reduction could be achieved. |
- Category
- HLS Constraints
- Value Type
- Integer
- Valid Values
- 0, 1
- Default Value
- As listed in the table above.
- Location Where Default is Specified
examples/legup.tcl
- Dependencies
- None
- Applicable Flows
- All devices and flows
- Test Status
- Actively in-use
- Examples
set_parameter LATENCY_REDUCTION 1