8-bit AVR Microcontrollers

Overview of the TWI Module

The TWI module is comprised of several submodules, as shown in the following figure. The registers drawn in a thick line are accessible through the AVR data bus.

Figure 1. Overview of the TWI Module