Low-Power Crystal Oscillator

This Crystal Oscillator is a low-power oscillator, with reduced voltage swing on the XTAL2 output. It gives the lowest power consumption, but is not capable of driving other clock inputs, and may be more susceptible to noise in noisy environments.

The crystal should be connected as described in Clock Source Connections. When selecting crystals, load capacitance must be taken into consideration. The capacitance (Ce+Ci) needed at each TOSC pin can be calculated by using:

Ce+Ci=2CLCs
where:
Table 1. Internal Capacitance of Low-Power Oscillator
32 kHz Osc. Type Internal Pad Capacitance (XTAL1) Internal Pad Capacitance (XTAL2)
Ci of system oscillator (XTAL pins) 18 pF 8 pF

The Low-power Oscillator can operate in three different modes, each optimized for a specific frequency range. The operating mode is selected by the fuses CKSEL[3:1], as shown in the following table:

Table 2. Low-Power Crystal Oscillator Operating Modes(1)
Frequency Range
 [MHz] CKSEL[3:1](2) Absolute Limits for Total Capacitance of C1 and C2 [pF](4)
0.4 - 0.9 100(3)
0.9 - 3.0 101 12 - 22
3.0 - 8.0 110 12 - 22
8.0 - 16.0 111 12 - 22
Note:
  1. 1.These are the recommended CKSEL settings for the different frequency ranges.
  2. 2.This option should not be used with crystals, only with ceramic resonators.
  3. 3.If the crystal frequency exceeds the specification of the device (depends on VCC), the CKDIV8 Fuse can be programmed in order to divide the internal frequency by 8. It must be ensured that the resulting divided clock meets the frequency specification of the device.
  4. 4.When selecting the external capacitor value, the stray capacitance from the PCB and device should be deducted. The total load (Ce+Ci+Cs) on XTAL pins must not exceed 22 pF.

The CKSEL0 Fuse together with the SUT[1:0] Fuses select the start-up times, as shown in the following table:

Table 3. Start-Up Times for the Low-Power Crystal Oscillator Clock Selection
Oscillator Source/Power Conditions Start-Up Time from Power-Down and Power-Save Additional Delay from Reset 
(VCC = 5.0V) CKSEL0 SUT[1:0]
Ceramic resonator, fast rising power 258 CK 19CK + 4 ms(1) 0 00
Ceramic resonator, slowly rising power 258 CK 19CK + 65 ms(1) 0 01
Ceramic resonator, BOD enabled 1K CK 19CK(2) 0 10
Ceramic resonator, fast rising power 1K CK 19CK + 4 ms(2) 0 11
Ceramic resonator, slowly rising power 1K CK 19CK + 65 ms(2) 1 00
Crystal Oscillator, BOD enabled 16K CK 19CK 1 01
Crystal Oscillator, fast rising power 16K CK 19CK + 4 ms 1 10
Crystal Oscillator, slowly rising power 16K CK 19CK + 65 ms 1 11
Note:
  1. 1.These options should only be used when not operating close to the maximum frequency of the device, and only if frequency stability at start-up is not important for the application. These options are not suitable for crystals.
  2. 2.These options are intended for use with ceramic resonators and will ensure frequency stability at start-up. They can also be used with crystals when not operating close to the maximum frequency of the device and if frequency stability at start-up is not important for the application.