8-bit AVR Microcontrollers

SPI Control Register 0

When addressing I/O registers as data space using LD and ST instructions, the provided offset must be used. When using the I/O specific commands IN and OUT, the offset is reduced by 0x20, resulting in an I/O address offset within 0x00 - 0x3F.

The device is a complex microcontroller with more peripheral units than can be supported within the 64 locations reserved in Opcode for the IN and OUT instructions. For the extended I/O space from 0x60 in SRAM, only the ST/STS/STD and LD/LDS/LDD instructions can be used.

Name:
SPCR0
Offset:
0x4C
Reset:
0x00
Access:
When addressing as I/O register: address offset is 0x2C
Bit76543210
SPIE0SPE0DORD0MSTR0CPOL0CPHA0SPR0 [1:0]
AccessR/WR/WR/WR/WR/WR/WR/WR/W
Reset00000000

Bit 7 – SPIE0: SPI0 Interrupt Enable

SPI0 Interrupt Enable

This bit causes the SPI interrupt to be executed if the SPIF bit in the SPSR register is set and if the global interrupt enable bit in SREG is set.

Bit 6 – SPE0: SPI0 Enable

SPI0 Enable

When the SPE bit is written to one, the SPI is enabled. This bit must be set to enable any SPI operations.

Bit 5 – DORD0: Data0 Order

Data0 Order

When the DORD bit is written to one, the LSB of the data word is transmitted first.

When the DORD bit is written to zero, the MSB of the data word is transmitted first.

Bit 4 – MSTR0: Master/Slave0 Select

Master/Slave0 Select

This bit selects the Master SPI mode when written to one, and the Slave SPI mode when written logic zero. If SS is configured as an input and is driven low while MSTR is set, MSTR will be cleared and SPIF in SPSR will become set. The user will then have to set MSTR to re-enable Master SPI mode.

Bit 3 – CPOL0: Clock0 Polarity

Clock0 Polarity

When this bit is written to one, SCK is high when idle. When CPOL is written to zero, SCK is low when idle. Refer to Figure 1 and Figure 2 for an example. The CPOL functionality is summarized below:

Table 1. CPOL0 Functionality
CPOL0 Leading Edge Trailing Edge
0 Rising Falling
1 Falling Rising

Bit 2 – CPHA0: Clock0 Phase

Clock0 Phase

The settings of the Clock Phase bit (CPHA) determine if data is sampled on the leading (first) or trailing (last) edge of SCK. Refer to Figure 1 and Figure 2 for an example. The CPHA functionality is summarized below:

Table 2. CPHA0 Functionality
CPHA0 Leading Edge Trailing Edge
0 Sample Setup
1 Setup Sample

Bits 1:0 – SPR0 [1:0]: SPI0 Clock Rate Select

SPI0 Clock Rate Select

These two bits control the SCK rate of the device configured as a master. SPR1 and SPR0 have no effect on the slave. The relationship between SCK and the Oscillator Clock frequency fosc is shown in the table below.

Table 3. Relationship Between SCK and Oscillator Frequency
SPI2X SPR0[1] SPR0[0] SCK Frequency
0 0 0 fosc/4
0 0 1 fosc/16
0 1 0 fosc/64
0 1 1 fosc/128
1 0 0 fosc/2
1 0 1 fosc/8
1 1 0 fosc/32
1 1 1 fosc/64